Smart and Sustainable Monitoring Solutions for Pneumatically Driven Machines

Pneumatics is the discipline that describes compressed air flow and how to use the properties of compressed air to transmit energy or convert the same into force and motion. Pneumatic applications use the most widely available resource — air. Pneumatic systems are integral to industrial automation and are especially useful when machines need linear motion or elastic behavior. It is also a functional way to store energy for subsequent uses.