This next generation ISE70 pressure sensor provides continuous quantitative values, as well as switched digital outputs when pressure set points are met.  This sensor is also IO-Link compatible.  Sensor information, such as identity, functional state, cable connection, and current or switch values can be set or monitored remotely though an IO-Link master, and connected to a fieldbus network.  The ISE70 is designed for abusive environments that may also include splashed coolant, lubricants or grime.  Electronics are packaged in a metal housing, while the piping connection is a stout lug with female threads, which together protect the sensor against accidental collisions with other objects in the area.  A smooth display face with membrane type buttons avoids contamination from grit and sticky residue that could clog or jam raised rubber buttons.  The display is angled and can rotate 336 degrees, to permit easy reading when indirectly mounted.  The main screen shows instantaneous values in red or green, while the sub screen setting appear in orange.  Switch indicators will also light when set points are reached.