Solutions to Wiring Problems

Wireless pneumatic solenoid valve interfaces
Electrical connections for pneumatic solenoid valve manifolds have developed over the years from individually wired solenoids to common cable solutions such as 25 pin D-sub connections, and then to fieldbus communications. This evolution has led to reduced installation time and reduced errors from incorrect wiring. Fieldbus communications have also enabled diagnostic feedback in addition to discrete and analog inputs common with the valve communications.